Technical FAQs

Ask a Question

Details Returned from IBM Devices via Advanced Device Crawlers

Issue:

Details Returned from IBM Devices via Advanced Device Crawlers

Product Line:

NetBotz

Environment:

NetBotz version 2 Advanced Device Crawlers.

Cause:

The following information can be queried via Advanced Device Crawlers for IBM systems assuming the IBM DDF (Device Definition File) is installed on the NetBotz appliance and the IBM system is SNMP enabled. Please note that not all information listed below is available on all IBM models.

Resolution:

 
  • Power Supply State
  • System Thermal State
Was this helpful?
What can we do to improve the information ?