Configuring SeaLevel 450 Relay I/O Device within Netbotz
Issue:
Configuring SeaLevel 450 Relay I/O Device within Netbotz
Product Line:
NetBotz Sealevel
Environment:
NetBotz version 2 and 3 Sealevel 450
Cause:
3rd party device configuration.
Resolution:
Once the I/O Device is connected to the Appliance, configuration for the Seal/O device can be done by the following:
1. Launch the Advanced View on the Appliance.
2. Double click the 'Serial Devices' Applet
3. In the drop-down menu, select the Sea-Level Product >> SeaLevel SeaI/O 450.
4. Then select 'OK'