Technical FAQs

Ask a Question

How to reboot the SmartConnect Network Interface

Issue:
How to reboot the SmartConnect Network Interface 

Product Line:
SmartConnect enable Smart-UPS

Environment:
Smart-UPS SMC, SMT, SRT with built in SmartConnect network port

Cause:
Need to reboot for X reason or need to establish connectivity or re-establish connectivity with SmartConnect cloud

Solution:
To reset the network interface of an SMT model UPS, on the display interface hold the UP and DOWN buttons simultaneously for 5 seconds. The display flashes to indicate that the network interface has restarted.
To reset the network interface of an SMC model UPS, on the display interface hold the MUTE and MENU buttons simultaneously for 5 seconds. The display flashes to indicate that the network interface has restarted.
To reset the network interface of an SRT model UPS, on the display interface hold the ENTER and ESCAPE buttons simultaneously for 5 seconds. The display flashes to indicate that the network interface has restarted.
 
Was this helpful?
What can we do to improve the information ?