Technical FAQs

Ask a Question

Can other manufacturer's cabinets be installed in the HyperPod?

Issue: 
Does HyperPod support other cabinet manufacturer's, or just APC NetShelter? 

Product Line: 
HyperPod 

Environment: 
All versions and serial ranges 

Cause: 
Customers may want to install a 3rd party cabinet into the HyperPod. 

Resolution:   
Yes, 3rd party cabinets can be installed in the HyperPod easily. Height differences are no problem with the adjustable brush strips that mate with the cabinet roof. 
Was this helpful?
What can we do to improve the information ?