Technical FAQs

Ask a Question

Video: How to confirm a good download file to upgrade StruxureWare Data Center Expert?

Issue:
How to confirm a good download file to upgrade StruxureWare Data Center Expert?

Product Line:
StruxureWare Data Center Expert
StruxureWare Central

Environment:
StruxureWare Data Center Expert all versions

Cause:
Prior to upgrading StruxureWare Data Center Expert it is always recommended that the upgrade zip file be checked for corruption. Otherwise, it is possible to corrupt the entire system while the upgrade process is running. Once the system is corrupted the only way recover to a working configuration is a complete restore and import of a backup. Please see "How do I backup StruxureWare Data Center Expert to a Windows share?" knowledge base for step by step instructions to create a backup on a Window machine.

Resolution:
The following video tutorial features a free MD5 Checksum program called WinMD5 that is readily available on the World Wide Web.

 
Was this helpful?
What can we do to improve the information ?