Technical FAQs

Ask a Question

Is there a kit available to convert from a NetShelter SX cabinet to a NetShelter SX Networking cabinet?

Issue:
A customer is requesting a kit to change the rails of a NetShelter SX cabinet into the SX Networking cabinet.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
The customer may have purchased the wrong cabinet or their needs may have changed.

Resolution:
There is currently no kit available to convert a NetShelter SX cabinet into a NetShelter SX Networking cabinet. The rails are not sold separately. There are more differences between the SX and SX Networking cabinets than just the rails. For a complete overview of the differences please see Knowledge Base article FA158652.
Was this helpful?
What can we do to improve the information ?