Technical FAQs
Technical FAQs
Issue:
What alarms can be automatically reset on a High Capacity Uniflair Unit
Product line:
High capacity Models 4500/5000
Environment:
All Serial Numbers
Cause:
Install
Resolution:
The Automatic Reset allows the unit to clear the alarm and continue operation if the alarm condition is no longer present.
• High/Low Temperature Threshold Exceeded
• High/Low Humidity Threshold Exceeded
• Supply Air Temperature Threshold Exceeded
• High/Low Airflow
• Humidifier
• Smoke Detected
• Electric Heater Over Temperature
• Electronic Expansion Valve Error
• Low Pressure
• Circuit 1 Chilled Water High Temperature Threshold Exceeded
• Circuit 1 Chilled Water Temperature too High for Dehumidification
• Insufficient Chilled Water Flow
• Primary/Secondary Power Source Unavailable
• Dual Circuit Expansion Board Error Detected
• Digital 2/4/6 Input Abnormal
• External Sensor Threshold Exceeded