Technical FAQs

Ask a Question

Details Returned from Alcatel Devices via Advanced Device Crawlers

Issue:

Details Returned from Alcatel Devices via Advanced Device Crawlers

Product Line:

NetBotz

Environment:

NetBotz version 2 Advanced Device Crawlers.

Cause:

The following information can be queried via Advanced Device Crawlers for Alcatel systems assuming the Alcatel DDF (Device Definition File) is installed on the NetBotz appliance and the Alcatel device is SNMP enabled. Please note that not all information listed below is available on all Alcatel models.

Resolution:
 
  • Description
  • Power Supply
  • Primary MPM Temp Sensor
  • Secondary MPM Temp Sensor
  • Fan Tray
Was this helpful?
What can we do to improve the information ?