BERMUDA - Choose Country or Region
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
Audio-Video Solutions
AV Power Conditioners with Battery
AV Surge Protectors
AV Power Filters
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
Room Cooling Accessories
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
iBusway for Data Center
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
Room Power Distribution
Cabinet Power Distribution
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
SmartShelter Room
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
Data Center Assessment Services
Install
Installation Services
Operate
Remote Monitoring Services
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
When to replace your battery or UPS
UPS Buying Guide
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
BERMUDA - Choose Country or Region
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
Version 1 Appliance Will Not POST to NetBotz Central 2.x
Issue:
Version 1 Appliance Will Not POST to NetBotz Central 2.x
Product Line:
NetBotz
NetBotz Central
Environment:
NetBotz version 1
NetBotz Central 2.x
Cause:
Troubleshooting posting issues.
Resolution:
First, browse to the bot in question and check the PICPOSTURL field:
http://ip-of-wallbotz/http.txt
If the \""PICPOSTURL\"" doesn't have the port specified, it's the standard port 80, otherwise it should be whatever follows the hostname of the NBC.
If you want to change the port or the hostname/IP of the NBC, you’ll type the following in the URL field of the bot:
http://ip-of-wallbotz/setHttp?PICPOSTURL=http://ip-or-hostname-of-nbc-server:PORT/central/photoman
Note: If the ports are correct, and the hostname is correct, make sure the appliance can resolve the hostname of the NBC. To do this, telnet to the appliance and do a \""gethostbyname nbc-server-name\"".