Technical FAQs

Ask a Question

Video: How to Start your Symmetra PX 250/500 UPS

Issue:
How to Start your Symmetra PX 250/500 UPS
 
Product line:
Symmetra PX 250/500
 
Environment:
All Product models, all serial numbers

Resolution:
Begin by applying power to the UPS by Closing the Q1 Breaker (Located in System I/O Cabinet)



Once the display is completely powered up and the Home screen is displayed, press the wrench icon in the lower left of the screen



Then select the operation button
Select System Startup



Follow the on screen prompts for starting up the UPS.  As each option is performed it will highlight the next step.


Some options are automated and will be done for you.

The following video demonstrates this procedure:
 
Was this helpful?
What can we do to improve the information ?