Technical FAQs

Ask a Question

Does the AR2144BLK or AR2145BLK NetShelter VX Seismic have leveling feet or castors available as an accessory?

A customer may ask if castors are an accessory for our NetShelter VX cabinet.

Product Line:
NetShelter VX 
All versions and serial ranges.
Some customers may wish to have a NetShelter VX cabinet with castors. 
Resolution :

The NetShelter VX cabinets do not offer castors as an accessory. These cabinets are approved for NEBS GR-63-CORE seismic installation, which does not include the use of castors.
Also see attached document.
Was this helpful?
What can we do to improve the information ?