Technical FAQs

Ask a Question

NetBotz post-only mode fails when entering only hostname of Central server.

Issue:
NetBotz post-only mode fails when entering only hostname of Central server

Product Line:
StruxureWare Central/Data Center Expert
NetBotz

Environment:
StruxureWare Central / Data Center Expert any version
NetBotz any version.

Cause:
Lack of DNS info or fully qualified name.

Resolution:
When entering server information into the "InfraStruxure Central IP/Hostname" field of the Advanced View POST-only-mode configuration window, you must enter either an IP for the Central server or it's fully qualified domain name. Entering in only the host name without the domain information will cause the posts to fail. Additionally, if you do not add the proper DNS entries into the NetBotz configuration, posting will fail as well.
 
Was this helpful?
What can we do to improve the information ?