Technical FAQs

Ask a Question

Empty gray screen appears when trying to run graph in ISX Central on a Windows 2000 system.

Issue:
Empty gray screen appears when trying to run graph in ISX Central on a Windows 2000 system

Product Line:
InfraStruxure Central

Environment:
Potentially every version (newer versions not tested on Windows 2000)

Cause:
APC has seen 2 instances where running a graph on a Windows 2000 system causes a blank window. In these cases, windows did not have the gdiplus.dll file installed

Resolution:
The file in question can be downloaded here:

http://www.microsoft.com/en-us/download/details.aspx?id=18909

Was this helpful?
What can we do to improve the information ?