Technical FAQs

Ask a Question

Sensor Specifications for Version 2 Netbotz Appliances

Issue:

Sensor Specifications for Version 2 Netbotz Appliances

Product Line:

NetBotz

Environment:

NetBotz version 2 sensors

Cause:

Sensor specifications.

Resolution:

Integrated Sensor Specifications:

Temperature sensor Range:
- 35F to 120F
- 1.6C to 48.8C

Temperature sensor Accuracy:
+ or – 1.8F
+ or – 1C

Humidity sensor Range:
- 10% to 90% non-condensing

Humidity sensor Accuracy:
+ or – 5% RH

Dew Point sensor Accuracy:
+ or - 2 degrees F

Airflow sensor Range:
- 40 fpm to 400 fpm

Airflow sensor Accuracy:
+ or – 50 fpm

Was this helpful?
What can we do to improve the information ?