Technical FAQs

Ask a Question

Severity Level is Incorrect in ISX Manager for High Temperature on External Sensor Violation Events

"These alarms are incorrectly mapped in the ISX Manager. The ISX Manager defines these events as ""Critical"" while the Network Management Card defines them as ""Warning"" level events. There is no workaround for this issue at this time other than to make sure that the appropriate notifications are set up for Warning and Critical Level Events. "
Was this helpful?
What can we do to improve the information ?