What is the difference between the leak sensors AP9325 and AP9326?
Issue:
What is the difference between the leak sensors AP9325 and AP9326?
Product line:
All InRow Units
Environment:
Data Center Cooling
Cause:
Resolution:
There are 3 main differences:
AP9325 is used for the Gen1 InRow RC , InRow SC, InRow RD, and Environment & Monitoring Systems, whereas the AP9326 is just for the Gen1 600mm InRow RP, RD, and RC
The AP9326 is the extension cable of AP9325.
The connection for AP9325 is RJ45, whereas the AP9326 connection is a 2 prong Molextm connector. Please see below: