Modular PDU Breaker LED Light Staying Green or Not Changing State
Issue:
Modular PDU Breaker LED Light Staying Green or Not Changing State
Product line:
Modular PDU
Environment:
Opening and closing of breaker does not change the LED status light on breaker
Cause: If the Modular PDU Alarm Status if set to Off, the breaker will never change state. So the Green LED will always be lit -> If the Modular PDU "Alarm Status" and "Position Alarm" is set to Off, the breaker will never change state. So the Green LED will always be lit
Resolution: In the Web interface of the PDPM, within the settings of each module, the “enable” box needs to be checked so the alarm and LED will trigger. The “Mass Configuration” option is available only when looking at the “all locations” screen. -> In the Web interface of the PDPM, within the settings of each module, both “enable” box needs to be checked so the alarm and LED will trigger. The “Mass Configuration” option is available only when looking at the “all locations” screen.