BAHRAIN - Choose Country or Region
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
Voltage Regulators
Surge Protection Devices
Filters & Harmonic Conditioners
Mobile Accessories
Portable Device Chargers
Cooling
Cooling
Cooling
Modular Access Floor
Uniflair Technical Floor
Uniflair Office Floor
Uniflair Building Floor
Air Economizers
Ecoflair Air Economizers
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
Static Transfer Switches
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
Module Optimized Cooling
Chilled Water System
Power Modules
Enclosed Power Module
Skid Mounted Power Module
IT Modules
SmartShelter Container
SmartShelter Module
SmartShelter Data Hall
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
Data Center Assessment Services
Install
Installation Services
Operate
Battery Replacement Services
Extended Warranties
Preventive Maintenance
Service Plans
Optimize
Training Services
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
BAHRAIN - Choose Country or Region
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
What is the cfm rating of the NetShelter CX with AR4703 installed?
Issue:
Customers want to know the cfm rating of NetShelter CX cabinets with the AR4703 fan booster installed.
Product Line:
NetShelter CX.
Environment:
All versions and serial ranges.
Cause:
Installing the AR4703 increases the cfm of the NetShelter CX cabinet.
Resolution:
18U with 1x AR4703 - 260 CFM
24U with 2x AR4703 - 330 CFM
38U with 3x AR4703 - 340 CFM