Technical FAQs

Ask a Question

Maximum Number of Netbotz Appliances or Sensors on a Graph within Netbotz Central.

Issue:

Maximum Number of Netbotz Appliances or Sensors on a Graph within Netbotz Central

Product Line:

Netbotz Central

Environment:

NetBotz Central 1.x and 2.x

Cause:

Software Limitations.

Resolution:

Maximum Number of Appliances or Sensors on a Graph

NetBotz Central 1.x only graph 11 appliances at once. If more than 11 appliances are selected, then only first 11 selected are graphed.

NetBotz Central 2.x does not have this limitation. It can generate graphs for different sensors of the same type for a single appliance or multiple appliances. However, the more sensors are selected for a graph, the more memory and processing power are required for the client running NetBotz Central console.

Was this helpful?
What can we do to improve the information ?