Technical FAQs

Ask a Question

NetBotz v2 | Why does Netbotz Advanced Device Crawlers show no environmental data on a Cisco 3524 Switch

Issue:
Why do Netbotz Advanced Device Crawlers show no environmental data on a Cisco 3524 Switch?

Product Line:
NetBotz (NB) v2 (320, 420, & 500)
NetBotz (NB) v3 (355, 355, 450, 455, 550, & 570)

Environment:
NetBotz
NetBotz Device Monitoring Pack (license)

Cause:
Cisco 3524 switch does not publish environmental data via the SNMP agent.

Resolution:

The Cisco 3524 switch does not publish environmental data via the SNMP agent, therefore; Netbotz Advanced Device Crawlers does not show any environmental information for the device.
Was this helpful?
What can we do to improve the information ?