Technical FAQs

Ask a Question

Enabling or disabling ISX Central Private LAN will cause server to generate a new self signed SSL certificate.

Issue:

Enabling or disabling ISX Central Private LAN will cause server to generate a new self signed SSL certificate

Product Line:

InfraStruxure Central

Environment:

InfraStruxure Central prior to 6.2

Cause:

When working with SSL certs, you will need to re-add the cert if you enable or disable DHCP on the private LAN or if you change IP information on the private LAN. This is a known issue.

Resolution:

This issue was resolved in InfraStruxure Central 6.2

Was this helpful?
What can we do to improve the information ?