Technical FAQs

Ask a Question

How to reset MGE SNMP/ Web card back to default MGE UPS

Issue:
Resetting MGE SNMP/ Web card back to default MGE UPS
 
Product line:
MGE Galaxy series UPS and MGE Multislot add on smart slots
 
Environment:
Galaxy 3000
72-170000-00:10kva small box, 72-170100-10:10kva large box
72-170100-00:15kva small box, 72-170200-10:20kva large box
72-170300-10:30kva large box, 72-171200-10: 20kva parallel,
72-171300-10:30kva parallel
Galaxy 4000
72-173005-00:40-50kva
72-173008-00:65-80kva
Galaxy 5000
72-174001-00:40-80kva
72-174002-00:100-130kva
72-174011-00:40-80kva parallel
72-174012-00:100-130kva parallel
Galaxy PW
72-130113-00:225kva
72-131113-00:225kva parallel
Multislot
66071
 
Cause:
none
 
Resolution:
See attached file named "Restoring the default password for SNMP.docx" for details
 

 
Was this helpful?
What can we do to improve the information ?