Technical FAQs
Technical FAQs
Issue:
Special characters can be used for password on a SNMP card
Product line:
SNMP card part#: 66074 or 34003640SE
All MGE UPS
Environment:
All model numbers/ all serial numbers
Cause:
Customer wanted to use special characters for password on a SNMP card for higher level of security. The login and password by default are: MGEUPS. Each field accepts up to 10 characters max.
Resolution:
Here are the special characters can be use for password ~ ! @ # $ % * ( )