Technical FAQs

Ask a Question

PowerChute Business Edition looses communications with HP ProLiant server

Issue:
PowerChute Business Edition loses communications with HP ProLiant server.

Product Line:
PowerChute Business Edition (PCBE)

Environment:
PCBE running on HP ProLiant server and communications method is serial

Cause:
HPs Integrated Lights-Out (iLO)

Resolution:
Please review HP Kbase
http://h20564.www2.hpe.com/hpsc/doc/public/display?docId=emr_na-c00843255&sp4ts.oid=398220
Was this helpful?
What can we do to improve the information ?