Is the AP9361 (Netbotz Rack Access PX - HID) compatible with VX racks?
Issue:
Is the AP9361 (Netbotz Rack Access PX - HID) compatible with VX racks.
Product Line:
NetBotz
Environment:
NetBotz rack access
Cause:
Compatibility
Resolution:
No. The AP9361 (Netbotz Rack Access PX - HID) is not compatible with VX racks. The AP9361 is only compatible with the SX and SV racks. The NetBotz rack access pod (NBPD0171) uses the same handle as the AP9361 and it too is incompatible with the VX racks.