Technical FAQs

Ask a Question

Power Over Ethernet (POE) and NetBotz version 1 or 2 Appliances

Issue:

Power Over Ethernet (POE) and NetBotz version 1 or 2 Appliances

Product Line:

NetBotz

Environment:

NetBotz version 1 and 2

Cause:

Alternative methods for powering NetBotz appliances.

Resolution:

None of the NetBotz Version 1 or 2 Appliances natively support Power Over Ethernet (POE). However, D-Link Corporation Linksys make POE adapters that will work with the following NetBotz Appliances:

Model 300
Model 303
Model 310
Model 320
Model 400
Model 420

The Model 500 requires more power than the POE standard supports and it also has a proprietary power connector.

Was this helpful?
What can we do to improve the information ?