Technical FAQs

Ask a Question

AP8xxx incorrect Hardware Revision number

Certain AP8xxx PDU's were manufactured with a different value in the "hardware revision" field 

Product Line
Rack Power Distribution - models starting with AP8xxx

Serial range prior to 0218

A small number of rack PDU's with serial number date range before 0218 may have an incorrect hardware revision value. Typically this field shows "02", however affected PDU's can show many different values in this field. This value is cosmetic only, and is used only for reference. The hardware revision value does not impact the function of a PDU.

Was this helpful?
What can we do to improve the information ?