Technical FAQs

Ask a Question

When finger-style vertical cable managers are used is it possible to also block off the openings in the mounting rails?

A customer using the finger-style vertical cable managers inside a NetShelter cabinet wants to know how to block hot air from recirculating through the rails.

Product Line:
NetShelter SX

All versions and serial ranges.

There are holes in the finger-style vertical cable managers to allow cables to run from front to rear inside the cabinet. If left open hot air can recirculate through these holes. 

When there are finger style cable managers installed inside the cabinet, AR7714 can be used as a pass-thru airflow management accessory. The AR7714 installs onto the finger style vertical cable manager. 

Without the finger-style vertical cable managers in place, AR7706 can be used in the wide NetShelter cabinets. It's a brush strip style airflow management product that allows cables to pass through. It installs onto the vertical mounting rail. 

Was this helpful?
What can we do to improve the information ?