Technical FAQs

Ask a Question

Can equipment be installed on the floor of a NetShelter CX or CX Mini?

Customers may ask if it's OK to install equipment on the floor of a NetShelter CX or CX Mini.

Product Line:
NetShelter CX
All versions and serial ranges.
Customer's equipment doesn't all fit into the U-space provided.
Before installing any equipment on the floor of the NetShelter CX please check with the OEM manufacturer for their installation recommendations.
The floor of the NetShelter CX and CX Mini is solid. There is no airflow being introduced from directly below the floor.
Was this helpful?
What can we do to improve the information ?