Technical FAQs

Ask a Question

Video: Back-UPS ES - Procedure for Battery Replacement

Issue:
Demonstration of the internal  battery installation for the BACK-UPS ES family.

Product Line:
BACK-UPS ES

Environment:
BE350G, BE450G, BE550G, BE650G, BE650G1, BE750G

Cause:
The internal batteries contained  in APC UPS' are shipped disconnected per DOT requirements.

Resolution: 
The following video details the process for accessing and removing the internal battery of a Back-UPS ES UPS.


Was this helpful?
What can we do to improve the information ?