Technical FAQs

Ask a Question

Are APC Cat 6 Patch Panels color coded for 568B or 568A?

Issue: 
The installer needs to know the color code on the rear of the Cat 6 patch panel.  
 
Product Line:
Cables and Connectivity Solutions, Patch Panels
 
Environment:
CAT6PNL-24, CAT6PNL-48
 
Cause:
Installers need to know if the patch panel has the color code they require.
 
Resolution :
see below

The CAT6PNL-xx series of Patch Panels have both 568B and 568A color codes. Cat 5e, 6 and 6a patch cables and other cabling accessories can be viewed at www.apccables.com 
Was this helpful?
What can we do to improve the information ?