Technical FAQs

Ask a Question

Models of Pelco cameras that have been tested with version 3 NetBotz and BotzWare 4.X

Issue:

Models of Pelco cameras that have been tested with version 3 NetBotz and BotzWare 4.X

Product Line:

NetBotz
Pelco Cameras

Environment:

NetBotz NBWL0455 and NBRK0570 
4.X botzware
Pelco camera support

Cause:

Not all Pelco cameras have been tested with NetBotz 4.0 botzware.

Resolution:

Please note that the NetBotz 3xx and NetBotz NBRK0450/0451 do not support the Pelco integration.


The initially supported Pelco cameras from version 3.x firmware are:
 
Pelco Camera Model Product Family Firmware Version Tested
IP3701H-2 IP Unavailable
IP110-CHV9 IP110 Camclosure® Unavailable
SD4N-W0 Spectra Mini IP Unavailable



The following is a list of cameras and Pelco firmware that has been tested with BotzWare version 4.0. The Sarix line of Pelco cameras have been added to testing:
 
Pelco Camera Model Product Family Firmware Version Tested
IXS0C Sarix IX 1.7.19.9080-A1.5842
IXE20DN Sarix Enhanced 1.7.19.9081-A1.5843
IX30DN Sarix IX 1.7.8.9080-A1.5288
IMSOC10 Sarix IME 1.7.41.9260-O2.6725
SD4N-W0 Spectra Mini IP  1.2.15

 
With the release of Botzware 4.2, the following list of additional Pelco cameras and firmwares have also been tested:
 
Pelco Camera Model Product Family Firmware Version Tested
IMSOC10 Sarix 1.8.2
IM10C10 Sarix 1.8.2
IX30DN Sarix IX 1.8.2
D5118 Spectra HD 1.8.2
TXB-N Spectra IV IP 1.8.2
DD4N-W0 Spectra Mini IP 1.2.15
IP110 IP110 Camclosure® 1.0.47
IP3701 IP 1.0.10

The following is a list of cameras and Pelco firmware that has been tested with BotzWare version 4.4:
 
Pelco Camera Model Product Family Firmware Version Tested
IM10C10 Sarix 1.9.2
IMS0C10 Sarix 1.9.2
D5118  Spectra HD 1.9.2
IME119 Sarix Enhanced 2.1.2.0.8280-A0.0

The following is a list of cameras and Pelco firmware that has been tested with BotzWare version 4.5.3:
Pelco Camera Model Product Family Firmware Version Tested
IL 10 Sarix Unavailable
 
The following is a list of cameras and Pelco firmware that has been tested with BotzWare version 4.5.4:
Pelco Camera Model Product Family Firmware Version Tested
IJP121-1IS
Sarix
01.16.17

Important Note:

Pelco Sarix Pro models that were originally listed as supported do not correctly update the resolution settings presented to NetBotz appliances. NetBotz can no longer support Sarix Pro models due to this limitation of the Pelco camera and they have been removed from this compatibility matrix.
 
 
Was this helpful?
What can we do to improve the information ?