Technical FAQs

Ask a Question

User name and password lengths for InfraStruXure Central and Netbotz appliances for an SNMP version 3 inform.

Issue:

User name and password lengths for InfraStruXure Central and Netbotz appliances for an SNMP version 3 inform.

Product Line:

NetBotz

Environment:

Netbotz SNMP v3

Cause:

SNMP version 3 requirements

Resolution:

v3 informs only work under certain circumstances.

md5/des user/password must be 8-15 characters
md5/aes user/password must be 8-15 characters
sh1/aes user/password must be 16+ characters
sh1/des user/password must be 16+ characters

for md5 the user name and password only work if they are between 8-15 characters.
for sh1 the user name and password only work if they are >16 characters.
Was this helpful?
What can we do to improve the information ?