Technical FAQs

Ask a Question

Details Returned from MGE Devices via Netbotz Advanced Device Crawlers

Issue:

Details Returned from MGE Devices via Netbotz Advanced Device Crawlers

Product Line:

NetBotz

Environment:

NetBotz version 2 Advanced Device Crawlers.

Cause:

The following information can be queried via Advanced Device Crawlers for MGE systems assuming the MGE DDF (Device Definition File) is installed on the NetBotz appliance and the MGE system is SNMP enabled. Please note that not all information listed below is available on all MGE models

Resolution:

 
  • Description
  • Receptacle
  • Battery Run Time Remaining (charge vs. load)
  • Remaining Battery Capacity
  • Battery Voltage
  • Battery Current
  • Battery Temperature
  • Battery Full Recharge Time (at current load)
  • Battery Fault
  • Battery Status Unavailable
  • Battery Needs Replacement
  • Battery Unavailable
  • Battery Not Fully Charged
  • Battery Low
  • Battery Charge Fault
  • Battery Low Condition
  • Battery Low Recharge Indicator
  • Utility Power Failure
  • Utility Power Failure Cause
  • UPS On Battery
  • UPS On Bypass
  • Bypass Unavailable
  • Bypass Not Installed
  • UPS in Battery Backup Time
  • UPS On Booster
  • Inverter Off
  • Output Overload
  • UPS Over Temperature
  • UPS On Fader
  • Ambient Temperature
  • Ambient Humidity
  • Temperature Sensor
  • Humidity Sensor
  • Last Self-Diagnostic Test Result
  • Last Battery Test Result
Was this helpful?
What can we do to improve the information ?