Technical FAQs

Ask a Question

Verifying Digitally Signed Pictures with Version 2 Netbotz Appliances

Issue:

Verifying Digitally Signed Pictures with Version 2 Netbotz Appliances

Product Line:

NetBotz

Environment:

NetBotz version 2

Cause:

NetBotz has included a simple command line utility that enables you to verify that digitally signed M-JPEG (AVI) files have not been tampered with since they were generated by your NetBotz appliance.

Resolution:


The file name of the command line utility is:
avivrfy.bat

It is automatically installed and can be accessed from the Advanced View installation directory.

Command Usage:
avivrfy avifilename.avi

To verify multiple AVIs,:
avivrfy sample.avi sample1.avi sample2.avi”

Was this helpful?
What can we do to improve the information ?