Technical FAQs

Ask a Question

Wireless Adapters Supported in the NetBotz 500

Issue:

Wireless Adapters Supported in the NetBotz 500

Product Line:

NetBotz

Environment:

NetBotz 500

Cause:

The following 802.11 PC Card slot adapters are supported in the NetBotz 500 (NBWL0500)

Resolution:



Adapter Part Number Wireless Protocols Cisco Leap Support
Proxim Orinoco Classic Gold 8410-WD 802.11b No
Cisco Aironet 350 PC Card AIR-PCM352 802.11b Yes
CiscoAironet 802.11a/b/g Wireless Cardbus Adapter AIR-CB21AG-A-K9
AIR-CB21AG-E-K9
AIR-CB21AG-J-K9
AIR-CB21AG-W-K9
802.11a/b/g No
D-Link Air Expert DWL-AG650 Cardbus Adapter DWL-AG650 802.11a/b/g No
NetGear WAG511 802.11a/b/g Dual Band Wireless PC Card WAG511 802.11a/b/g No


The following GPRS / GSM PC Card slot adapters are supported in the NetBotz 500
Option International GlobeTrotter
Sierra Wireless AirCard 750
Sierra Wireless AirCard 775
Sierra Wireless AirCard 850/860
Xircom CreditCard Modem 56-GlobalACCESS
 
recently added:
Sierra Wireless AirCard 850/860
http://www.sierrawireless.com/product/ac860.aspx
http://www.sierrawireless.com/product/ac850.aspx

Option GlobeTrotter 3G QUAD
http://www.option.com/products/globetrotter_3G_QUAD.shtml

Option Globesurfer ICON USB (HSDPA/UMTS/EDGE/GPRS/GSM)
http://www.option.com/products/globesurfer_icon.shtml

MultiModem GPRS USB (non-USB interface versions not supported)
http://www.multitech.com/PRODUCTS/Families/MultiModemGPRS/

MultiModem EDGE USB (non-USB interface versions not supported)
http://www.multitech.com/PRODUCTS/Families/MultiModemEDGE/

Was this helpful?
What can we do to improve the information ?