Technical FAQs

Ask a Question

Uniflair PCO1 Cool Setpoint Reverts to 0

Issue:
Uniflair PCO1 Cool Setpoint Reverts to 0

Product line:
Uniflair

Environment:

Cause:
Cool Setpoint revert to 0

Resolution:
If the cool setpoint reverts to 0 or another value after setting it through the front screen, remove all communication (web, modbus, ect) connections. These have the ability to change the setpoints and can cause it to revert to a different setpoint if not set up properly.

Was this helpful?
What can we do to improve the information ?