InfraStruXure Central 6.0 shows un-localized text in Server Administration Settings Time Zone drop down box when using Brazilian Portuguese or Russian.
Issue:
InfraStruXure Central 6.0 shows un-localized text in Server Administration Settings Time Zone drop down box when using Brazilian Portuguese or Russian.
Product Line:
InfraStruXure Central
Environment:
InfraStruXure Central 6.0 and higher
Cause:
Due to a bug in Java, the Time Zone drop down box in ISXC 6 console will not show as Brazilian Portuguese or Russian. This defaults to English.