Technical FAQs

Ask a Question

How can I change my pump rollover timer settings in my Motivair pump package?

Issue:
How can I change my pump rollover timer settings in my Motivair pump package?
 
Product line:
All Motivair Dry Coolers Eaton 500 PLC controllers
 
Environment:
All Serial Numbers
 
Cause:
Install, Repair
 
Resolution
 
This controller can be changed through the display
 
Setting Changeover Timers:
The changeover timer is set with the buttons on the front of the Easy Relay.  Changeover is measured in Hours.  To adjust the Changeover timer, press OK, then use the Up or Down arrows to highlight Parameter.  Press OK and O1 is selected.  Press OK again.  The first digit in O1 is selected.  Press OK again.  The cursor changes to a blinking digit.  Press the right arrow to move the cursor over to the digit to be changed.  Use the Up or Down arrows to adjust the value of the selected digit.  Once the desired changeover time has been set, press OK, then press Esc three times.
 
 
NOTE: Factory Default Program has a 7-day (168 hours) pump rotation/changeover timer setting.
 
 
Was this helpful?
What can we do to improve the information ?