Technical FAQs

Ask a Question

Are there Gender Changers that have opposite genders, like DB25 male/female?

There may be need for an adapter that has a male connector on one end and a female connector on the other.

Product Line:
Cables and Connectivity Solutions

All versions and serial ranges.

These help lengthen the life expectancy of a port that experiences a high rate of connecting and disconnecting cables.

Yes but they are not really Gender Changers. They are typically called Port Protectors or Port Extenders. They can be used to help lengthen the life expectancy of a port that is repeatedly connected to. They can also be used to add height to a recessed port.

All APC brand Cables and Connectivity Solutions products like Cat 5E, Cat 6, Cat 6A patch cables, fiber optic cables, USB cables and adapters, Monitor cables, A/V cables, adapters and converters can be found at: 
Was this helpful?
What can we do to improve the information ?