Technical FAQs

Ask a Question

Updating Firmware to APC devices from InfraStruXure Central fails when updating 350 or more nodes.

Issue:

Updating Firmware to APC devices from InfraStruXure Central fails when updating 350 or more nodes.

Product Line:

InfraStruxure Central

Environment:

InfraStruxure Central any version
APC SNMP devices and firmware updates.

Cause:

When updating the firmware APC devices from InfraStruXure Central, you can select specific nodes to upgrade.

Resolution:

APC recommends selecting a lower amount of devices to update such as 100 nodes at a time.

Was this helpful?
What can we do to improve the information ?