Details Returned from Extreme Networks Devices via Advanced Device Crawlers
Issue:
Details Returned from Extreme Networks Devices via Advanced Device Crawlers
Product Line:
NetBotz
Environment:
NetBotz version 2 Advanced Device Crawlers.
Cause:
The following information can be queried via Advanced Device Crawlers for Extreme Networks systems assuming the Extreme Networks DDF (Device Definition File) is installed on the NetBotz appliance and the Extreme Networks system is SNMP enabled. Please note that not all information listed below is available on all Extreme Networks models.