Duplicate IP addresses listed in InfraStruXure Manager
"When a device is moved from one InfraStruXure Manager Network to another InfraStruXure Manager Network, it may retain the IP address it was assigned by the original InfraStruXure Manager. This may result in two devices having the same IP address in the user interface of the second InfraStruXure Manager. To resolve this, reboot the Network Management Card of the newly added device and InfraStruXure Manager will then issue a different IP address to the rebooted device. The duplicate IP address will still remain in the user interface of InfraStruXure Manager in a ""Lost Communication"" state until it is manually deleted."