Technical FAQs

Ask a Question

Can troughs install across the rear of the new NetShelter roof?

Issue: 
It appears that troughs can't install across the rear of the NetShelter roof. 

Product Line:
NetShelter SX

Environment: 
AR3100, AR3300, AR3150 

Cause: 
Some of the trough mounting holes are missing. 

Resolution: 

Troughs can also be installed by connecting them to the adjacent trough. Please see page 1 of the Installation Instructions.  
Also, see the attached file. 
Was this helpful?
What can we do to improve the information ?