Technical FAQs

Ask a Question

Does the W870-8135 NetShelter key work on the combination handle AR8132A?

A customer claims that their new AR8132A door handles can be opened with the standard NetShelter 333 key: W870-8135. 

Product Line: 
NetShelter SX, AR8132A

All models, all serial numbers. 

The AR8132A uses a different key, but the standard 333 key will also open the lock. 

The AR8132A will accept any key similar when the combination is set to the factory default of 000. 
Once a new combination is set, only the key included with the AR8132A will open the lock. 
Was this helpful?
What can we do to improve the information ?