Technical FAQs

Ask a Question

How to change the Inroom’s unit of measurement

Issue:
How to change the Inroom’s unit of measurement 

Product line:
InRoom, Stulz, ACPDX21-86, ACPCW40-150 

Environment:
All Product models, all serial numbers 

Cause:
Change unit of measurement

Resolution: 
You can adjust the temperature display in °C or °F 
Operate > System > temp.unit > change from C/F 
Some fw versions may have you select Operate > System > AT-Preferences as seen below

 
 
 
The corresponding IOC commands:
unit c / unit f
language e / language g
 
NOTE:            c for °Celsius, f for °Fahrenheit, e for English, g for German
 
Was this helpful?
What can we do to improve the information ?