Technical FAQs

Ask a Question

"ISX Central's Internal Browser ""Home"" button doesn't work with 2.x NMC Firmware"

Issue:

ISX Central's Internal Browser ""Home"" button doesn't work with 2.x NMC Firmware

Product Line:

InfraStruxure Central / Struxureware Data Center Expert.

Environment:

InfraStruxure Central / Struxureware Data Center Expert
Any version 2.x firmware on APC SNMP enabled devices.

Cause:

Any APC device running older 2.x firmware reacts differently due to coding differences.

Resolution:

There is no plan to update this feature at this time to work with the older devices.

Was this helpful?
What can we do to improve the information ?