Camera flicker filter not available in Netbotz advanced view with some cameras.
Issue:
Camera flicker filter not available in Netbotz advanced view with some cameras.
Product Line:
NetBotz
Environment:
NetBotz version 2 and 3 cameras
Cause:
Older version 2 camera pod 150 units had the flicker filter option under the camera configuration capture option. Newer camera pod 150 units with a revision of A2 will not show this option.
Resolution:
These cameras can be identified in the Advanced View by going to the about tab and looking for the revision. A camera pod with a revision with A0 should show this option. The version 3 camera pod CP160 will also not have this option available.