Technical FAQs

Ask a Question

Serial Terminal Connection Parameters for all NetBotz Appliances

Issue:

Serial Terminal Connection Parameters for all NetBotz Appliances

Product Line:

NetBotz

Environment:

Versions as described below
terminal emulation

Cause:

Terminal emulation (ie. Hyper-Terminal) configuration for communications with NetBotz appliances.

Resolution:

Terminal emulation is often used for initial IP configuration on NetBotz appliances. Hyper-terminal or Putty are often used for this configuration.
 

Serial Terminal Connection Parameters for all NetBotz Appliances

When connecting to a Netbotz appliance or a NetBotz Central via a serial cable, the terminal settings must be set to:

38400 and 8-N-1

When connecting to a models 300, 303, 310, or 400, you must use a standard serial cable, such as the kind used to connect a modem to a PC.

When connecting to models 320, 420 or 500, you must use a NULL modem cable.

When connecting to models 355, 455, 550, 570 or similar version 3 Netbotz, you must use a USB A-B cable.

The NetBotz 200 uses a Null Modem cable and a baud rate of 9600.

NOTE: When connecting to a NetBotz Central, you must use a NULL modem cable.
 

Was this helpful?
What can we do to improve the information ?