Technical FAQs

Ask a Question

Video: How to change the Display password Timeout settings on a Network Air FM unit

Issue:
How to change the Display password Timeout settings on a Network Air FM unit
 
Product line:
FM 35-50, IR40, ACFM400, ACFM200
 
Environment:
All Serial Numbers
 
Cause:
Install, Configuration
 
Resolution:

 
  1. Press the ESC Key until you get to the main menu
  2. Press ENTER on Setup
  3. Press ENTER on System 1
  4. Press ENTER on Display
  5. Press ENTER on Password & Timeout
  6. Using the UP or DOWN arrows you can select the Timeout (This will allow the amount of time on the display before you will have to enter a password again)
  7. Press ENTER and now you will need to enter a password
  8. The default password is 7852 Select each number and then press ENTER to move to the next one
  9. Press ENTER again and you can change the time from 1 min to 4 hours
  10. Press ENTER and the ESC back to the status menu
  11. Finish by pressing the ENTER key and then press ESC until you get to the status menu
Was this helpful?
What can we do to improve the information ?